4/12/2016 1:35 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello SIMATIC Ident RFID systems FB 45 for MOBY U, MOBY D, RF200, RF300 Function Manual et200 pro and RF170c hw configuration Why does the RFID standard block FB45 / FC45 report "error_bus 80A2" when using an RF170C? |
There is no such thing as the last bug in a program |
|
4/13/2016 11:36 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating:
|
If you are using TIA Portal V13 SP1 or greater you can use the build in ident blocks. You can find then at the instructions window at "Optional packages". You can find a manual for those blocks here: Or is it STEP 7 Classic you are using? |
This contribution was helpful to
1 thankful Users |
Follow us on