12/12/2023 11:31 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
yes you need a seperate licence for WinCC Unified PC |
12/12/2023 11:47 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
afaik no, for PC Runtime no TRIAL Licence |
12/12/2023 11:19 PM | |
Joined: 10/12/2023 Last visit: 1/31/2025 Posts: 31 Rating:
|
|
No such thing as a stupid question |
|
1/1/2024 6:04 PM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello Nkuthal, Part A:
Part B: Now if you have any of the below non-WinCC Unified licenses then still the respective Unified license is compatible, and the respective Unified device(s) can be configured and used in TIA Portal.
Part C: If you have installed the WinCC Unified software and do not have license, then you have the one-time option of activating a Trial License. However, this license is valid for a limited period only and expires after 21 days. Please refer the Licensing STEP 7 and WinCC section in the V18 System Manual for all these details. Hope this helps. If you have any further questions, please feel free to ask. Thank you!! |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on