10/3/2011 5:28 PM | |
Joined: 5/4/2009 Last visit: 5/28/2024 Posts: 914 Rating:
|
Dear friend, One last question, If we have one LOGO! acts as master and two others acts as slaves, how can the master distinguish between I/Os coming from first slave and I/Os coming from the second? Regards. Tomy
|
Aim Higher |
|
10/4/2011 8:17 AM | |
Joined: 9/30/2005 Last visit: 7/15/2024 Posts: 42 Rating:
|
Tomy, Each LOGO has another IP adress. So you can distinguish from witch LOGO the I/O's are comming. Hope this helps. |
10/4/2011 8:18 AM | |
Posts: 2930 Rating:
|
Hi, the IP-Address of the slave seperates the units. Regards |
4/24/2014 7:46 AM | |
Posts: 340 Rating:
|
new question is splittet to How many digital and/or analog inputs and outputs, can be used with a master or slave logo. |
This contribution was helpful to
1 thankful Users |
5/20/2014 7:24 AM | |
Posts: 340 Rating:
|
new question is splittet to how to set up the mapping (eg. Local VB0 Remote IB0) 2 LOGO!´s |
This contribution was helpful to
1 thankful Users |
Follow us on