Industry Online Support
Technical Forum
1/6/2011 5:36 PM | |
Posts: 65 Rating: (0) |
hello sir, i am not able to link SFC and CFC which i created in the process cell.Can u tell me the procedure for that??? |
1/7/2011 9:00 AM | |
Posts: 86 Rating: (7) |
Keep in mind with SFC you use (type or single) and it also not possible to connect a struct to the SFC. Yer |
1/7/2011 9:50 AM | |
Posts: 288 Rating: (22) |
If you want to control some variables from the SFC, Phantom has given you every thing you need to know. If you want to control certain phases of the SFC itself based on some logic, You can follow these steps. 1) Open the SFC. 2) Inthe Menu: View -> External View This opens the SFC like a block in a dedicated CFC. Here You can interconnect the SFC Parameter like Auto Start, Stop , Hold, Abort etc... like any other blockbetween 2 CFC's AttachmentSFC_CFC_INTERCONNECTION.zip (93 Downloads) |
Last edited by: Yoga Shankar at: 1/7/2011 9:51 AM |
|
This contribution was helpful to1 thankful Users |