Now the application exampleis availableSINAMICS G:Speed Control of aG120/G120C/G120D using S7-300/400 (STEP 7 V5)with PROFINET/PROFIBUS and Safety Integrated (via PROFIsafe) and HMI
supplemented with the new CU250S-2andFW V4.6
10/18/2012 6:32 PM | |
Joined: 10/26/2011 Last visit: 3/14/2023 Posts: 766 Rating:
|
Hello PCS 7 Users, Now, there is a Page available, which shows you all application and engineering examples for SINAMICS G and SINAMICS S drives. The sample applications provide: |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
8 thankful Users |
2/7/2013 1:40 PM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Now you can find here www.siemens.com/sinamics-applications a scalable web page of application examples for SINAMICS S, SINAMICS G, SINAMICS V and other drives. You can set the filters in combination with drive type, PLC, communication type between drive and PLC, drive function and so on. |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
This contribution was helpful to
3 thankful Users |
4/5/2013 11:09 AM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Now it's availableSINAMICS S: Positioning of a S120 using S7-300/400 (STEP 7 V5) with PROFINET/PROFIBUS, Safety Integrated (not via PROFIsafe) and HMI. The application shows you the positioning of several axes of a SINAMICS S120 with PROFINET or PROFIBUS connected with a SIMATIC S7-300. The safety functions of the SINAMICS S120 are controlled via terminals. The FB283 for EPOS control and a HMI for user control is used. You can donwload the application here Link. Here you can find all applications for SINAMICS S120 Link. |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
This contribution was helpful to
1 thankful Users |
4/24/2013 3:12 PM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Now it's availableSINAMICS G: Speed control of a G120 using S7-300/400 (TIA-Portal) with PROFINET/PROFIBUS and Safety Integrated (not via PROFIsafe) and HMIThe application example shows you the control of a SINAMICS G120 with PROFINET/PROFIBUS using a SIMATIC S7-300 PLC in TIA-Portal You can download the application example for STEP 7 V11+SP2 or STEP-7 V12. Here you can find the application example Link. All application examples for SINAMICS G120 you can find here. |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
5/15/2013 10:14 AM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
The application examples for the new SINAMICS CU250S-2 are available now. SINAMICS G: Positionig a G120 CU250S-2with S7-300/400 (STEP 7 V5)via PROFINET/PROFIBUS using Safety Integrated (via PROFIsafe)and HMI SINAMICS G:Speed control of aG120/G120C/G120D/G120Pwith S7-300/400 (STEP 7 V5)via PROFINET/PROFIBUSusing Safety Integrated (not via PROFIsafe) and HMI You can find all SINAMICS G120 application exampleshere. |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
This contribution was helpful to
1 thankful Users |
6/19/2013 11:09 AM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Now the application exampleis availableSINAMICS G:Speed Control of aG120/G120C/G120D using S7-300/400 (STEP 7 V5)with PROFINET/PROFIBUS and Safety Integrated (via PROFIsafe) and HMI |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
This contribution was helpful to
2 thankful Users |
6/24/2013 12:22 PM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Hallo together, |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
6/24/2013 12:30 PM | |
Joined: 1/13/2009 Last visit: 1/26/2023 Posts: 35 Rating:
|
Here a collection of helpfulSINAMICS S120 DCC application examples |
Weitere SINAMICS Applikationen unter www.siemens.de/sinamics-applikationen |
|
6/24/2013 12:57 PM | |
Posts: 35 Rating:
|
Dear speedychecker1: I almost shed tears of joy when I saw this post Thank you guys for sharing this whole thread Best Regards, M.Gad |
Follow us on