3/5/2023 3:19 AM | |
Joined: 12/18/2014 Last visit: 6/29/2024 Posts: 33258 Rating: (4115)
|
No. The web server doesn't have a database in which to permanently store the values. |
3/8/2023 10:48 AM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating: (207) |
Here is an example for a bucked chains storage as Ella_68 has mentioned. Each value of the chain can be used in the web browser as little bargraph to show e.g. a trend for the last 4 or more hours. Just expand the chain for an amount as needed, if there is enough space for the program. Regards, Scorp AttachmentBucked Chain Storage1.zip (379 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on