11/16/2013 11:19 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, which memory module is plugged? On a EPROM you can not write via transfer, you must use a prommer. If you want to test it without write the memory module you must use a RAM-module if the memory in the PLC is not enough. If you are searching for mudules you can contact me. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
Follow us on