7/8/2020 1:05 PM | |
Joined: 10/11/2006 Last visit: 5/2/2024 Posts: 5831 Rating: (789)
|
Hello, depending on the dynamic requirements, you could use just the second motor with droop (not the positioning or leading motor), or you use the application and setup droop and compensation if the second motor gets too weak in dynamic operation. I would not recommend an analogue coupling of the torque value, as this may lead to vibrations due to noisy signals, but you could also try this. |
With best regards, |
|
7/10/2020 11:21 AM | |
Joined: 8/3/2011 Last visit: 3/21/2024 Posts: 100 Rating: (7) |
Thanks a lot.....I will experiment a little then.... |
Follow us on