Industry Online Support
Technical Forum
11/30/2009 10:36 AM | |
Posts: 45 Rating:
|
Hi! If u want to disable auto detect on hardware u should stop and disable "Plug and Play" in Services (Start > Control Panel > Administrative Tools > Services). Right click on plug and play and click on properties to change those settings. Other services u should disable is following: -Windows Firewall -Universal Plug and Play Device Host -Removable Storage -Plug and play Properties -Automatic Updates Disable auto popup for cleaning desktop wizard..http://support.microsoft.com/kb/320154 That would turn off the most of windowsautomaticallypopups. To access wincc explorer or windows desktop u can look on this thread:/tf/WW/en/Posts/22236 |
Last edited by: ÅF-Patrik at: 11/30/2009 10:39 AM |
|
11/30/2009 10:40 AM | |
Posts: 134 Rating:
|
also disable Sticky Keys(SHIFT pressed 5 times in a row) in Control panel-->Accesibility options |
11/30/2009 12:42 PM | |
Joined: 8/11/2008 Last visit: 4/8/2024 Posts: 67 Rating:
|
hi. i also use a microsoft tool called Tweak UI (that can be downloaded here) to improve the solutions above. with this tool you can, for instance, disable "Win+X" keys (you know, Win+D to show desktop, Win+E to open windows explorer and so on...), disable the "logoff" button in start menu and, the most important in my point of view, disable autorun for every device (dvd drive, usb drive....) among other system features. also, you can take a look in microsoft support page "How can I prevent users from connecting to a USB storage device?" if you need to allow some users to backup data using external hdds. best regards |
Roger A. Manrique |
|
This contribution was helpful to
1 thankful Users |
11/30/2009 1:16 PM | |
Posts: 38 Rating:
|
Thanks a lot for your useful & practical ideas! |
Follow us on