7/6/2020 11:25 AM | |
Posts: 27 Rating: (0) |
Hello all. I have a similar question regarding the possibility of logging when a certain bit is triggered. I have 5 real values and 2 strings that I would like to log when a trigger bit is set to ''1''. Is this possible in WinCCflex (TIA PORTAL V14). I've entered the variables in the Log configuration, set the acquisition mode to ''On Demand'' (is this correct) and now I don't know where to set which bit executes one ''log cycle''. Please give me some feedback if this is possible to do, and any pointers on how to propper configure it would great. Cheers. Aleix
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2020 12:47:39New subject after splitting |
|
Follow us on