3/1/2017 11:11 AM | |
Posts: 215 Rating: (6) |
[Split from another thread] When using S7, I can create a log file including name and value of the variables. I tried to make a similiar file using OPC. I can get the IOT to log the value of the variable, but it doesn't include the name of the tag in the file. Is there any way to make it do this? ------------------------------------------------------------------------------------------ |
Last edited by: JDarius at: 3/1/2017 11:11:36 AMLast edited by: JDarius at: 3/1/2017 11:24:47 AMLast edited by: Min_Moderator at: 3/1/2017 11:49:40 AMNew subject after splitting Last edited by: Min_Moderator at: 3/1/2017 11:51:24 AMDelete answer of different thread |
|