12/2/2020 7:23 PM | |
Posts: 3 Rating: (0) |
Hello I am running a SCADA system and need the user to lock up after 3 attempts. I wait and you can help me Thank you
|
12/3/2020 8:46 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello E.Y94, you could use the option Simatic Logon, then the users
Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/7/2020 7:46 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello E.Y94, without Simatic Logon you can only create an own scripting see FAQ: https://support.industry.siemens.com/cs/ww/en/view/19141675 part "Procedure in SIMATIC LOGON up to version V1.2" "PWRTSilentLogin" is an ODK-function, there are some other ODK-functions,
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on