5/15/2018 2:14 PM | |
Posts: 11 Rating: (0) |
I have encountered a problem with FS6 (FW 1.81.03). The web server does not update the TDE display correctly: the cursor keys are not shown on the screen so it is not possible to browse through the messages. I have tested with Chrome, Opera and IE with similar results. The problem seems similar to earlier FS4 and FS5 problems described in Product information on LOGO! 8 FS:04 and FS:05 to errors The only way to restore normal operation was to power cycle Logo. Has anyone noticed similar behavior? |
5/16/2018 4:17 AM | |
Posts: 24 Rating: (4) |
is there AccessTool and other web browser is connected to LOGO ? the connection is limited. |
5/16/2018 7:46 AM | |
Joined: 12/18/2014 Last visit: 8/11/2024 Posts: 33528 Rating: (4166)
|
Start a Support Request. |
5/22/2018 12:11 PM | |
Posts: 11 Rating: (0) |
Update 2: The problem reappeared in another Logo with FW 1.81.03 (FS:06). I managed to get some screenshots with browser console open showing some error messages. I have sent the screenshots to Siemens for analysis and am waiting for their reply. I also had a look at the forum in German and someone else seems to have detected similar problem: Die Steuerung stürzt nach zirka 50 Tagen ab. |
This contribution was helpful to1 thankful Users |
Follow us on