2/6/2012 4:06 PM | |
Posts: 378 Rating: (73) |
Dear dears, My client have LOGO 230RC with display, 8 Digital Inputs and 4 Digital Outputs. When I first look, no program on the LOGO so I wrote the program from the machine sequence (because I dont have the source code). I wrote the program on LOGO soft comfort by ladder diagram ( Just for simulation), I dont have interface cable so i converted and wrote on the keypad (control pannel). Then the program works fine and everything is as I expected. I attached here my program. My problems is after I turn off the power for one day and turn on, one line of the program at the Q1 is changed to I1-----[ Q1 I correct check all the system then i turn off the power for 10 min and turn on everything is fine but when i turn off for one day and turn on, the same problem happens at Q1. Could you please tell me how this problem happens? I get confused how only one line of the program is lost? thank you! AttachmentCircuit Diagram1.zip (192 Downloads) |
2/7/2012 5:36 PM | |
Posts: 378 Rating: (73) |
The order code is 6ED1 052-1FB00-0BA4 and around 5 yealrs old. Am still with this problem, Any suggestions? |
Last edited by: desmul24 at: 2/7/2012 5:40 PM |
|
2/8/2012 5:20 PM | |
Posts: 378 Rating: (73) |
Dear Marcjan, Thanks for your help! I choose to train operators to write the program every time when it fails, rather replacing! |
Follow us on