12/24/2016 12:17 AM | |
Joined: 10/26/2013 Last visit: 7/22/2024 Posts: 47 Rating:
|
If you want to supply the Logo from the same powersupply, you do can use only one circuitbreaker. Remind though that the max of the extention contacts is 4A and you dont need to drive much power, so i suggets to use a 2A fuse or automatic circuitbreaker. For troubleshooting purpose sometimes its better to use more circuitbreakers, like: I normaly use fuseholders (and accessories) like: http://www.conrad.com/ce/en/product/1164259/Fuse-terminal-8-mm-Screws-Configuration-L-Grey-ABB-1SNK-508-410-R0000-1-pcs? |
Last edited by: JdZ at: 12/24/2016 12:18:16 AM |
|
This contribution was helpful to
1 thankful Users |
12/25/2016 4:48 AM | |
Posts: 2 Rating:
|
Thanks JdZ That was very helpful! |
Follow us on