11/28/2022 8:39 AM | |
Joined: 12/18/2014 Last visit: 8/12/2024 Posts: 33539 Rating: (4166)
|
Have you installed the driver for the original Siemens USB cable? |
11/28/2022 7:56 PM | |
Joined: 12/18/2014 Last visit: 8/12/2024 Posts: 33539 Rating: (4166)
|
The LOGO! 24R is a LOGO! of the first generation (year 1996). To connect to the PC you have to set this LOGO! in transfer mode. There are two ways. See attachment. AttachmentLOGO! 0BA0 Long manual page 108.pdf (377 Downloads) |
This contribution was helpful to2 thankful Users |
12/1/2022 7:00 PM | |
Joined: 6/7/2021 Last visit: 1/9/2023 Posts: 4 Rating: (1) |
Thanks for the information, the problem is solved. |
This contribution was helpful to1 thankful Users |
Follow us on