10/22/2021 9:58 PM | |
Joined: 3/2/2016 Last visit: 1/9/2025 Posts: 72 Rating: (14) |
Hi A_EIT, 6ED1055-1MM00-0BA2 is the AM2 AQ module for LOGO!8. You can check it in the LOGO! manual. Hope it helps! |
10/23/2021 5:05 AM | |
Joined: 12/18/2014 Last visit: 1/24/2025 Posts: 34557 Rating: (4313)
|
Since the delivery release of the first LOGO! 0BA8 (8/29/2014) there are also new expansion modules. They are to be used with all corresponding base modules of all 0BA8 series, as the older expansion modules are not compatible with base modules of the 0BA8 series. The new expansion modules all have the ending 0BA2 in the article number. Look here: Delivery Release for LOGO! 8 and LOGO! Soft Comfort V8 |
Follow us on