5/6/2022 7:34 AM | |
Joined: 9/11/2014 Last visit: 9/6/2024 Posts: 750 Rating:
|
Hi, try like in the picture: If your scale give the value 12.123KG = 12123 in LOGO!, then this should work with a resolution of 1g. For a display of the value you need analog amplifier to define how to display what you want. This should work till 32755 = 32.755kg 1:1. You can check in the simulation. Open the datatable to enter the values from your scale (left side in the picture) Important is that your scale give the value 1:1 als float. Then you can use the F/I-FB with a resolution of 1.000. In this case LOGO! just translate from float to Integer. The accepted range is the LOGO! integer range till 32755, which is 32.755kg. Hope this helps. Attachmenta_Wight.zip (454 Downloads) |
Follow us on