5/28/2019 11:04 PM | |
Joined: 11/3/2016 Last visit: 4/28/2024 Posts: 9 Rating: (0) |
Hi Ixo65. We are aware about the more or less 60 s resolution, and as we are using counters for cycles from 90 min to several hours, so it is not a problem at all. The issue is weird, as according our customer that is using two identical systems with same LOGO program, issue affect only the first counter of each logo, the two others ones seem to work. I attached the program. Any advice is welcome. Thanks.
AttachmentlogoPrg.zip (231 Downloads) |
5/29/2019 10:04 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32965 Rating: (4075)
|
For the LOGO! 8.2 (6ED1052-1MD08-0BA0) there has been a firmware update since 14 May 2019. Notes on instructions for updating the LOGO! 8.2 SP1 operating system |
5/29/2019 11:07 AM | |
Joined: 11/3/2016 Last visit: 4/28/2024 Posts: 9 Rating: (0) |
Ok. I will try to update. But right now I need to wait the authorization to download export restricted software. |
5/29/2019 11:09 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32965 Rating: (4075)
|
But do not get impatient. It may take a few days. |
6/8/2019 3:41 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32965 Rating: (4075)
|
Very strange mistake. Is not known to me. Maybe you should create a Support Request. |
Follow us on