9/9/2016 5:22 PM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33385 Rating:
|
Which color shows the LED on the expansions module? Red? Yellow? Or Green? |
9/9/2016 5:24 PM | |
Joined: 4/25/2014 Last visit: 5/15/2023 Posts: 11 Rating:
|
Green, unit is in Run and i can enter online test. |
9/9/2016 7:27 PM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33385 Rating:
|
With a Logo 230VAC you not make 24VDC on Input, only 115-230VAC on Inputs. |
9/9/2016 7:43 PM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33385 Rating:
|
The exact specifications please refer to the attachment.
AttachmentLOGO! 8 Soft manual 0BA8 2014_06.pdf (153 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on