11/15/2019 3:17 PM | |
Joined: 2/22/2008 Last visit: 11/18/2024 Posts: 2698 Rating:
|
If you have an appropriate flow meter or a level converter, then you can try the attached program. You need fast counter inputs, see technical data of your Logo. In my example I1 is the start signal and I3 is the sensor input. Q1 is for your solenoid. Don't change the direct connection between the sensor and the cnt input of the counter, this is required for fast counting. Regards, Scorp AttachmentFlowmeter1.zip (992 Downloads) |
This contribution was helpful to
1 thankful Users |
12/18/2020 10:25 AM | |
Joined: 12/18/2014 Last visit: 2/15/2025 Posts: 34692 Rating:
|
Why? Take a look at the technical datas of the LOGO!. AttachmentLOGO! 8 manual 0BA8 2014_06 pages 305+306.pdf (891 Downloads) |
Follow us on