7/11/2019 8:16 PM | |
Joined: 7/16/2016 Last visit: 9/7/2021 Posts: 8 Rating: (0) |
Hi I am trying to use a logo and the access tool to create a production count system that will give the operators live data. I have ran into a few issues with the logging, I have selected the data to be logged every 60 second but this increases by a few seconds every time my counters reset for some reason. The other issue is with the time stamp, I have my program setup to reset the counters on the hour, 15 minutes past, 30 minutes past and 15 minutes to the hour but this is being logged up to two minutes late at times so it screws up my spreadsheet i have attached some data collected as an example. I though it was maybe because the logo and collecting PC had the time set slightly different but i synced the time from the PC to the logo and still had the same issue, would a gps NTP server help with this issue? Thank you Craig AttachmentTEST_10.19.160.41_20190709163911.pdf (150 Downloads) |
Last edited by: c3ham at: 07/11/2019 20:21:20 |
|