4/22/2019 9:38 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072)
|
I make a test with anlog signal. I connected the AI1 of the base modulewith a controllable 0-10V signal and configured this in LOGO! program as PT100 / 1000 in the analogue amplifier. The output value of the analogue amplifier was mapped to the VW0 and the values of VW0 were logged (see video by link). [snip] AttachmentAccess Tool.zip (607 Downloads) |
Last edited by: ixo65 at: 4/22/2019 9:39:52 AMLast edited by: Jen_Moderator at: 4/24/2019 6:26:03 AMRemoved link and added file as an attachment. |
|
This contribution was helpful to4 thankful Users |
4/24/2019 3:59 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072)
|
Did you have a look at the operating instructions for the Access Tool? If you want more lines, you need to create a log file. This is then a CSV file and can store several variables in separate columns per log line. A CSV file can hold 20,000 lines. AttachmentLOGO! Access Tool Help_en_US.pdf (530 Downloads) |
10/27/2022 6:03 PM | |
Joined: 4/28/2020 Last visit: 3/12/2024 Posts: 27 Rating: (3) |
I can't manage to see the trend values. I did pretty much the same in the video in previous post, just changing the variable length from VW0 to VD0 as it is mapped in my configuration. See attached image. Murillo Gumiero |
Murillo Gumiero |
|
10/27/2022 6:26 PM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072)
|
Read my post once again. I wrote: LOGOVARLS ("VW0","TD") And all in capital letters ... |
10/28/2022 2:17 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072)
|
By me it works without problems ... |
Last edited by: ixo65 at: 10/28/2022 02:39:32 |
|
Follow us on