2/9/2016 12:47 PM | |
Joined: 5/27/2015 Last visit: 7/31/2024 Posts: 93 Rating: (1) |
Hello , can i use logo 8! and vsd sinamics V20 to control motor 3p 0.37kw? Thank you |
2/9/2016 1:25 PM | |
Joined: 3/28/2015 Last visit: 1/10/2025 Posts: 722 Rating: (214) |
Hello, You can use the analogue signal from LOGO to control VSD Sinamic V20 |
Eng.Mohamed Ibrahim |
|
2/9/2016 7:49 PM | |
Joined: 3/28/2015 Last visit: 1/10/2025 Posts: 722 Rating: (214) |
Hello, 1-The analogue signal 0-10V from LOGO connected to the terminals of the VSD "AI1 and 0V" or "AI2 and 0V" to control the motor speed. 2- The enable"start" DI signal to VSD from LOGO or any other device. 3-You can install a potentiometer in the terminals of the VSD"10V,AI1 and 0V" to control the motor speed. |
Eng.Mohamed Ibrahim |
|
Follow us on