7/29/2013 5:34 PM | |
Posts: 2930 Rating: (432)
|
Hi, have you enabled port forwarding for port 10001? |
7/29/2013 8:47 PM | |
Posts: 3 Rating: (0) |
Hi, I will try, Thanks. |
7/30/2013 8:07 AM | |
Posts: 2930 Rating: (432)
|
Hi, to your questions: PW: No, there is no PW protection part of the App. The PW has to be enabled in the router. Also VPN can be implemented. Web-Server: No, there is no Web-Server available for LGOO!. You can use a Siemens Comfort Panel. All Siemens Comfort Panles has a Web-Server you can use together with LOGO!. Siemens has presented this at the past main fairs with LOGO! 0BA7 and Comfort Panels. Control Input. You can never controll Inputs from any remote device because an Input will always be overwritten by the status of the physical input at a controller. But you can control an digital network input with the app. In the LOGO! program you use the digital network input like an input onboard. See the manual for the LOGO! App. Add the Vx.y adress of your digital network input into the Monitor table. Then you can control it from a smart phone. LOGO! App for Windows smartphones is not available from Siemens. Check the market place for windos phones to see if someone has developed a App for LOGO!. Hope this helps |
This contribution was helpful to1 thankful Users |
9/23/2013 4:02 PM | |
Posts: 2930 Rating: (432)
|
Hi, I have an Samsung XCover I with Android V2.3. Attached is a screenshot. Good luck |
12/11/2013 8:01 AM | |
Posts: 2930 Rating: (432)
|
Hi, you can do via a common WLAN Router. This is how I do it. Regards |