5/17/2010 1:52 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
ok here it is sorry Fred AttachmentLogodataLogger2010a.zip (1178 Downloads) |
This contribution was helpful to10 thankful Users |
5/19/2010 3:52 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Just a little info you can not run the logo software and the logger at the same time. Fred |
6/2/2010 11:13 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
i will look into this and get back to you by the weekend. Fred |
6/5/2010 4:50 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
PETER, I fixed the issue with the flags and it now works.see the revised logger. fred AttachmentLogodataLogger2010aREVISED.zip (751 Downloads) |
This contribution was helpful to1 thankful Users |
6/5/2010 9:42 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Good afternoon everyone, I used the data logger on an analog project and the logger recorded the analog values. I was using percentage.I will experiment with temperature next. Fred AttachmentLogodataLogger2010aANALOG.zip (697 Downloads) |
This contribution was helpful to1 thankful Users |
6/6/2010 12:41 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Sorry for another change , i added a reset button to the logger.So now you can reset back to row 11 with one push of the button. Fred AttachmentLogodataLogger2010aANALOG.zip (736 Downloads) |
Last edited by: derf nedraw at: 6/6/2010 1:04 AMLast edited by: derf nedraw at: 6/6/2010 12:41 AM |
|
This contribution was helpful to2 thankful Users |
6/6/2010 11:19 AM | |
Posts: 21 Rating: (0) |
Hello again, and thanks for your work. Unfortunately I still can’t log my flags. I have attached my program so you can see what I’m looking for. In the bottom right corner there are two flags (M1 and M2) that indicate the status of my valve in this solar heating setup. One flag if the valve is open and one flag if the valve is closed. But in the file both M01 and M02 shows “0” at all times. Am I looking at the wrong ID? AttachmentPool_controler.zip (788 Downloads) |
Follow us on