7/13/2013 2:42 PM | |
Posts: 378 Rating: (73) |
Hello Faranak, LOGO red module is a programming module with retention and know-how protection 1, if you installed this module you can not transfer2 the values of the hours counter. This module is applied for LOGO 0BA1, 0BA2 and 0BA3. [img=100x100] https://support.automation.siemens.com/WW/llisapi.dll/csfetch/4027969/P_ST70_XX_00757i.jpg [/img] For the red module see this link Please tell us your LOGO type? 1 know-how protection is a way of protecting your program source code from being read (seen) by another unintended persons. 2 To tranasfer the value of hour counter for connected LOGO device: Tools -> Transfer -> Hours Counter Use this menu command to read the hours counter of the connected LOGO! [img=394x239] /tf/WW/en/postattachments/download?attachmentId=38494 [/img] Regards, |
Last edited by: desmul24 at: 7/13/2013 3:17 PMLast edited by: desmul24 at: 7/13/2013 3:09 PM |
|
This contribution was helpful to1 thankful Users |
7/14/2013 10:00 PM | |
Posts: 378 Rating: (73) |
Hello Faranak,
Transfering hours counter means reading the current ( actual values ) from the device. If you remove the red module you have removed your program thus you can not read the values of hours counter because your hours counter are on the program (your program on memory card (red module)).
If you starter with LOGO, I suggest you to select the latest OBA7. It has many new features, like Ethernet Interface (you dont need extra adapter or special cable to interface, upload, download or monitor), UDF (User Defined Functions), Easy networking b/n LOGO devices ... a lot more new features compared to the old one. Here is the new LOGO 0BA7 manual. Hope Helps, |
This contribution was helpful to1 thankful Users |
2/2/2014 3:17 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
Follow up question published by JaviXis split to a seperate Thread with the subject LOGO! Hours Counter - Write initial number to the hours counter different from zero Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on