7/22/2016 10:07 PM | |
Joined: 12/18/2014 Last visit: 7/29/2024 Posts: 33437 Rating: (4153)
|
For the arrangement of the expansion modules and addressing, see attachment.
AttachmentLOGO! 8 Soft manual 0BA8 2014_06_side29.pdf (429 Downloads) |
This contribution was helpful to1 thankful Users |
7/22/2016 10:10 PM | |
Posts: 116 Rating: (2) |
Hello, So we change the modules with the same no. of input or output with the same signal type. |
7/22/2016 10:14 PM | |
Posts: 116 Rating: (2) |
Hello, What happen if we replace digital module 8 input with another digital module 16 input? |
7/22/2016 10:22 PM | |
Joined: 12/18/2014 Last visit: 7/29/2024 Posts: 33437 Rating: (4153)
|
Two adjacent DM8 you can replace it with a DM16. It needs to be changed in the program nothing.
AttachmentReplacing.pdf (245 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on