10/21/2015 7:24 AM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33787 Rating: (4195) |
I once created a simple project. You can choose between the logos to connect pervade create a line. Then double-click the connection line and it opens the connection table. When using the VB-addresses you need only make sure that these are not the two numbers. AttachmentConnection.wmv (237 Downloads) |
Follow us on