7/11/2023 10:12 AM | |
Joined: 7/11/2023 Last visit: 7/11/2023 Posts: 1 Rating: (0) |
Hi, We have an issue with LOGO software where it does not allow us to select the calibrated temperature sensor range0 to 50°C and only allows0 to 48°C stating “The measurement range determined by gain/offset is invalid. Used measurement range 0 to 48”. If I play around with Gain and Offset Parameter the minimum and maximum fixed range given is2 to 50°C. Please see document attached with relevant screenshots, could you please advise? Thank you. AttachmentLOGO! PI-Controller Issue.docx (387 Downloads) |
7/12/2023 8:44 PM | |
Joined: 12/27/2006 Last visit: 6/6/2024 Posts: 1197 Rating: (113) |
Is your sensor 0 - 50 degrees and 0 - 10 Volt? Try: Gain 0.05 and Offset 0 Make your programm in FBD, NOT in LD (Ladder) Attachment0-50.zip (369 Downloads) |
Last edited by: Toeternietoe at: 07/12/2023 20:45:29Last edited by: Toeternietoe at: 07/12/2023 20:47:18 |
|
Follow us on