12/26/2010 9:49 AM | |
Posts: 15 Rating: (1) |
you have to specify what are the I/O in your project KR |
12/26/2010 10:23 AM | |
Posts: 4 Rating: (0) |
HiAMIRRAZI: thanks for your reply first. the I/O assign list as below output/input note state I1 start button N.O. I2 reset button N.O. Q1 valve A N.C. Q2 valve B N.C. I push the start button(momentary push button), then the valve A and B act according to the program. use reset button i hope to reset the timer to zero. |
Last edited by: plectrum at: 12/26/2010 10:23 AM |
|
12/27/2010 6:33 AM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
take a look at the program maybe it help you AttachmentFORUM.zip (252 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
12/27/2010 8:23 AM | |
Posts: 4 Rating: (0) |
Hicdrshort thanks for your reply first. your program is ok ,but the A and B valve have a different time to opened or closed. you can check thesequencediagram as below. thanks |
12/27/2010 11:41 AM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
sory first one is not coreckt check this one adjust the timers to the time you need .( values are small only for test purpose ) AttachmentFORUM1.zip (286 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
12/27/2010 12:17 PM | |
Posts: 153 Rating: (15) |
Hi_plectrum мay be it in the attachment. 255s = 4 m 15 s 210s = 3 m 30 s You can change time in blocks with an inscription a step. Attachmentsolenoid valve.zip (277 Downloads) |
12/28/2010 6:25 AM | |
Posts: 4 Rating: (0) |
Hi cdrshort &Andrey [Str]: thanks for your program, it'sOK. thank you very much.
|
Last edited by: plectrum at: 12/28/2010 6:25 AM |
|
Follow us on