7/24/2018 4:58 PM | |
Posts: 439 Rating: (108) |
Hello, I am currently trying to send a analog setpoint from IOT2040 to a Logo! 0BA8 via S7 node of Node-red. This is not a Logo! 0BA8 FS4, so Modbus is not an option. I have seen couple post about Logo! to IOT communication, but can't find the perfect configuration. Please Help: IoT 2020 and Logo!8 Guide IoT2040 Various Communication Protocols Tested Do I need to create a S7 connection using TSAP or using RACK/SLOT or both of them works? Let's say I can see my connection is establish at some point. Which variable should I use in the Logo!, network analog input? How to write them on both side? I will let you know how it went. Best regards, HugoD |
7/24/2018 5:13 PM | |||||
Posts: 439 Rating: (108) |
Hello, I will base myself on the following example for communication between Logo! and S7-1200. Application examples for LOGO!
Will let you know any development. Have a good day! Best regards, HugoD |
||||