3/31/2023 2:20 PM | |
Joined: 12/20/2022 Last visit: 1/2/2024 Posts: 3 Rating: (0) |
Hello/Bonjour/Guten Tag, My copy of LOGO! Soft Comfort V8.3 suddenly stopped working. It happened to me late last year, and I was able to get it running, but now it seems I have the same problem again. I don't completely recall what I did to get it running again and the original installation DVD has been lost to time ever since we moved a couple of times. Older versions of the program (V8.2 V8.1 and V7) still run smoothly, but ever since converting those files to the latest hardware version, I can't open them in the older programs. Whenever I try to start the latest version, the splash screen shows briefly, but nothing happens. I've included a video showing.... well not much. I really hope anyone can help me out with this, we've got some big projects coming up and I really need to continue programming everything. Some technical info, in case it helps: With kind regards, Jasper AttachmentLOGO-Soft-Comfort-not-working.mov (739 Downloads) |
3/31/2023 2:26 PM | |
Joined: 12/18/2014 Last visit: 9/16/2024 Posts: 33779 Rating: (4194)
|
If you have also installed a older version of LSC on your PC, then can you upgrade to the current version 8.3. The to the upgrade find you here: Download links for current LOGO! software and firmware |
3/31/2023 2:48 PM | |
Joined: 12/20/2022 Last visit: 1/2/2024 Posts: 3 Rating: (0) |
I tried that but it didn't work either. It still gives me a brief flash of the splash screen and then nothing. |
4/3/2023 12:26 AM | |
Joined: 12/18/2014 Last visit: 9/16/2024 Posts: 33779 Rating: (4194)
|
The manual says: Windows 7, Wondows 8 and Windows 10. See attachment. If I were you, i would start a Support Request. AttachmentLOGO! 8 manual 0BA8 2022_07 xxxx8-0BA1 page 318.pdf (630 Downloads) |
6/4/2023 9:33 PM | |
Joined: 8/19/2014 Last visit: 4/29/2024 Posts: 10 Rating: (0) |
Hey Nardix, I have the same problem. Is it solved ? And when it is how did you do it ? best regards Nico |
Follow us on