5/2/2022 9:31 AM | |
Joined: 3/22/2018 Last visit: 5/28/2024 Posts: 17 Rating:
|
It does not go to the password menus . The TD logos are new and opened from the inside of the carton. AttachmentLOGO TD.zip (660 Downloads) |
5/2/2022 9:37 AM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33423 Rating:
|
This is new for me. Start a Support Request. |
This contribution was helpful to
1 thankful Users |
5/4/2022 10:39 AM | |
Joined: 9/19/2018 Last visit: 6/28/2024 Posts: 384 Rating:
|
OK, but if I do the same as in the video with my LOGO!TDE it works. Therefore I still think the two parts are defect. |
5/4/2022 12:12 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33423 Rating:
|
By my TDE (first generation) works it also with no problems. |
Follow us on