5/18/2017 10:17 PM | |
Posts: 6 Rating:
|
Hi all, I am a student working on a project using the Logo!8. I am new to the world of PLCs. We are trying to use the LOGO!8 with a tablet for a larger display using VTScada. We were advised to use the LOGO connected to a local wireless router via ethernet. From there, we will use a Lenovo IdeaStick to run VTScada and then use a tablet to display. The Lenovo and tablet will be accessed wirelessly using the router. This will all be mounted on a tractor and powered by a dedicated 12v battery with an inverter. While I understand this in concept, can someone please help me with execution? I have made my display with Scada, but the dials/gauges are not assigned. I am still working on making a program in Soft Comfort for the LOGO to interpret all the sensors that will be connected, but I do not know how to make the program work with VTScada. Any and all thoughts/advice/instruction would be much appreciated! Cait |
Last edited by: Cait at: 5/18/2017 10:25:49 PM |
|
5/19/2017 4:36 AM | |
Joined: 12/18/2014 Last visit: 8/25/2024 Posts: 33614 Rating:
|
I believe that will not work. In the driver list of Siemens devices the LOGO! not listed. The LOGO! 0BA8 (depends on the hardware version (FSxx)): - 0BA8.Stand (FS01-FS03): The best thing will be when you contact VTScada and ask you if the LOGO! can communicate with VTScada. AttachmentDatasheet-VTScada-DriverList.pdf (144 Downloads) |
Last edited by: ixo65 at: 5/19/2017 4:37:31 AM |
|
5/30/2017 8:04 AM | |
Posts: 2930 Rating:
|
Hi, here is a very simple LOGO! 8 program you can use to control Q1 of LOGO! from any SW witch is able to connect via S7-protocol to a LOGO! 8. Please set IP of LOGO! as you need. Try to control V0.0 from your SW. If everything is right, then Q1 on LOGO! can be controlled. By the way one failure any beginner makes is trying to control inputs. But inputs cannot be controlled. You can only READ inputs. Hope this helps AttachmentV0_0.zip (145 Downloads) |
Follow us on