7/2/2018 9:43 PM | |
Posts: 6 Rating: (0) |
Hi I am having difficulty changing the size of the analog value in LWE, it stays the same (about size 12). I tried to change the size in the main HTM-file, but i am not very familiar with HTML coding. I have added a screenshot of the web interface and the entire LWE file in a zip (i kept it very simple since this i my only problem so fare). Is there a easy way to do this? Martin AttachmentAnalog_reader_180702.zip (399 Downloads) |
7/3/2018 3:56 AM | |
Posts: 1283 Rating: (105) |
Can you try the attached file and see whether it works? Jay
Attachmentmain_test.zip (344 Downloads) |
7/3/2018 7:31 AM | |
Posts: 6 Rating: (0) |
Thanks, but it is still very small numbers in the analog value field (see attached picture). |
7/3/2018 11:28 AM | |
Joined: 10/20/2015 Last visit: 7/13/2024 Posts: 94 Rating: (19) |
Hello mkaastad369, Try the following,
|
7/3/2018 2:06 PM | |
Joined: 10/20/2015 Last visit: 7/13/2024 Posts: 94 Rating: (19) |
Try the following syntax, < font color="red"> or whatever color you want. |
Follow us on