9/19/2010 5:18 PM | |
Posts: 9 Rating: (0) |
When u say open connector u mean an open contact??? cause that makes no sense |
10/5/2010 8:17 PM | |
Posts: 9 Rating: (0) |
So i have the program right here guys. It is a simulation of a part of a productive fermentation where we got a main bottle getting filled up with mixtures of the other 2 bottles and after this is done we got mixing in the main bottle.Right after we got(i do not know the exact word of it) a moving way having on it the empty bottles that are going to be filled up with the mixture of the main bottle.And this fermentation is repeated right after with the same steps.Of course we got sensors and all that for the controlability of the whole. I got the program attached.Hope you will help me out.If u need extra info on the I/O of the system i'll just note them down for you.Just let me know. Thank you. Attachmentkanoniko me errors.zip (348 Downloads) |
10/9/2010 9:49 AM | |
Posts: 9 Rating: (0) |
We are using version 6 and i am not really sure i understand why we can't M1 flag may not be used and why those Inputs are not supported... |
Follow us on