Industry Online Support
Technical Forum
4/25/2019 4:03 PM | |
Joined: 8/10/2017 Last visit: 10/4/2024 Posts: 3 Rating: (0) |
Is it possible to connect and read values of an absolute encoder 6FX2001-5WN13 to Logo! v8 with ethernet port? |
4/25/2019 4:14 PM | |
Joined: 12/18/2014 Last visit: 1/25/2025 Posts: 34557 Rating: (4313)
|
Hello paakem, at first welcome to the forum. Not in my opinion. The device is designed for PROFINET IO, a field bus. But if you want an official statement from Siemens, start a Support Request. |
Follow us on