1/26/2015 4:16 PM | |
Posts: 46 Rating: (0) |
Dear All is it possible to use LOGO7 AI on LOGO8 unit? Best regards
|
1/26/2015 4:20 PM | |
Joined: 4/24/2006 Last visit: 1/24/2025 Posts: 8808 Rating: (1177) |
Hello, No, that is not possible, see the following link: Delivery Release for LOGO! 8 and LOGO! Soft Comfort V8 (See compatibility) Best regards, Wizard |
This contribution was helpful to1 thankful Users |
1/26/2015 9:04 PM | |
Joined: 12/18/2014 Last visit: 1/24/2025 Posts: 34557 Rating: (4313) |
Take a look at the attached PDF file, Side 2. Read the yellow marked text.
AttachmentSiemens Industry Online Support - Automation Service, Automation Support, Si.pdf (203 Downloads) |
1/27/2015 6:27 AM | |
Posts: 5225 Rating: (1198) |
..I did not bookmark the posting ..it is under [LINK] somewhere. It is safe to assume that the "experiment" I refered to has failed or is not practical - a German speaker answered here already. Better you go back to your product source and try and get something worked out in getting the right hardware. You should be able to still get OBA6 or OBA7 CPUs without price penalty.. The other day I even got an OBA5 from Siemens supplied as if an OBA6. - - and yes even the OBA5 works with the same expansions as the OBA6 and OBA7. Good luck. |
Follow us on