Industry Online Support
Technical Forum
9/30/2011 10:17 AM | |
Posts: 2930 Rating: (432)
|
Hi, you can use GSM-Modems. This modem must have digital inputs and then you need to configure if there is an pos. signal on one of the inputs to send a SMS to a modile phone. There are lots of this modem on the market. www.insys-tec.de for exapmle. Based on the missing serial interface at the LOGO! 0BA7 this is the only way I know. Hope this helps |
This contribution was helpful to1 thankful Users |
10/1/2011 7:20 AM | |
Posts: 153 Rating: (15) |
Hi, I think it there will be a good decision for my project of system of water protection. |
Follow us on