3/15/2022 9:13 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
You need not to insert the CMR module as a S7 compatible Modul in the network view. You must the CMR say in the CMR configuration that the CMR connected to the LOGO! 8.3 and their IP address. And also you have more to configure. See attachment. AttachmentIndustrial Ethernet LOGO! CMR2020 _ LOGO! CMR2040_Edition_2021_06.pdf (525 Downloads) |
This contribution was helpful to1 thankful Users |
3/16/2022 4:09 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
So you can read in the PDF that I attached before. I would say: Read the actual manual. You can download the actual manual from here: SIMATIC NET: LOGO! - Industrial Ethernet, LOGO! CMR2020, LOGO! CMR2040 |
Follow us on