5/5/2020 5:35 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33756 Rating:
|
By your LOGO! is it not possible to make a firmware upgrade. LOGO!s with the firmware versions V1.08.xx can't upgraded. AttachmentVersions of 0BA8.txt (267 Downloads) |
This contribution was helpful to
2 thankful Users |
5/5/2020 10:50 PM | |
Joined: 8/15/2015 Last visit: 8/21/2024 Posts: 133 Rating:
|
Dear Sir, Thank you, I didn't even saw that ...:'( What are my options? lastly is there a thread for feature requests? I would really like to see what expansion modules are connected on the CPU Thank you in advance |
5/5/2020 10:59 PM | |
Joined: 8/15/2015 Last visit: 8/21/2024 Posts: 133 Rating:
|
Also If I am willing to buy a new one to get the new features , How should I know if the Logo I am getting is the newest version or an old one ? |
5/6/2020 3:41 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33756 Rating:
|
You can recognize the current LOGO! 8.2 by the order number. Siemens has changed the order number system. Under this link you can download the free update to LSC V8.2.1: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) If you have Windows as the operating system, start the setup as an administrator. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 pages 363+364.pdf (235 Downloads) |
5/6/2020 6:44 AM | |
Joined: 9/11/2014 Last visit: 9/6/2024 Posts: 750 Rating:
|
Hi, at the packaging you can also find the ordernumber, the firmware version and the required LOGO! Soft Comfort version. So you don't need to open the pack and can identify if it the latest one. |
5/6/2020 3:36 PM | |
Joined: 8/15/2015 Last visit: 8/21/2024 Posts: 133 Rating:
|
Dear All , okay thank you for everything [snip] Thank you Le Test !! |
Last edited by: Jen_Moderator at: 05/07/2020 06:09:53Division of answers into separate topics. |
|
5/7/2020 6:08 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Le Test !! is split to a separate thread with the subject When order the new version , the old expansion modules also work ?. Best regards |
Follow us on