3/15/2022 10:50 PM | |
Joined: 4/28/2015 Last visit: 4/5/2022 Posts: 2 Rating: (0) |
When I try to connect I get a 'cannot access the remote device. I have uploaded screen shots of the error and settings.
AttachmentLOGO.docx (251 Downloads) |
3/16/2022 3:20 AM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33880 Rating: (4214)
|
Which LOGO! have you exactly? Please write the complete article number. If you have the current LOGO! 8.3 then need you LSC V8.3. The upgrade for free can you download from here: Download for LOGO! 8.3 Software UpgradeBut note: Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
3/16/2022 3:20 PM | |
Joined: 4/28/2015 Last visit: 4/5/2022 Posts: 2 Rating: (0) |
I have the logo 8 fs4. I registered to download lsc 8.3 last week, but I have not received conformation yet. |
3/16/2022 3:31 PM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33880 Rating: (4214)
|
FS4 is not enough. Please write the complete article number. |
Follow us on