4/21/2020 8:24 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820)
|
Hello, for this HW you need (in this time) MicroWin 4.0 SP9 as last version of SW. Last OS what is accepted is Win 7, also Win XP can be used without problems. In case you have PG yo can use internal MPI/DP port with PPI/MPI or PB DP protocol selected, then you can make test with connection to PLC. In other case (also OS play role here) some USB-PPI adapter can be used. Here is link to System manual: S7-200 System manual |
Last edited by: Duris_I at: 04/21/2020 20:26:13Last edited by: Jen_Moderator at: 04/22/2020 10:37:11Optimized link. With best regards... |
|
4/21/2020 10:41 PM | |
Joined: 9/27/2006 Last visit: 9/16/2024 Posts: 12282 Rating: (2684) |
Hello Mike; In addition to Duris_I's isuggestions, here are the part numbers of the software (S7-Microwin v4.0, now with SP9), and hardware (USB PC Adapter A2) that you will need to connect to and pogram a S7-200 PLC. Most of the information you need to upload, download program and modify the S7-200 you will find in the manual proposed by Duris_I. It is a most complete document. The USB PC Adapter A2 is not described as released for PPI communications (the S7-200 programming port communicates over PPI). The version of this cable is a replacement the original USB PC Adapters that were used a few years ago, and are now discontinued. This FAQ explains the issue: What should you watch out for with the PPI/MPI/DP interfaces if you want to use the CP 5711 / PC Adapter USB A2 with a SIMATIC S7-200? https://support.industry.siemens.com/cs/ww/en/view/85669627 Hope this helps, Daniel Chartier |
Follow us on