9/2/2021 9:33 AM | |
Joined: 11/24/2015 Last visit: 6/13/2022 Posts: 24 Rating: (0) |
I am looking for an example project for TP177A. I cannot find it in demo example. If some one can give me an example project. To modify it and download it to my tp177a. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/02/2021 13:17:55New subject after splitting |
|
9/13/2021 3:01 PM | |
Joined: 8/3/2009 Last visit: 9/6/2024 Posts: 13594 Rating: (1720)
|
Hello naceurmans I would use a demo project from: https://support.industry.siemens.com/cs/ww/en/view/22900091 Use a Basic Panel 1st Gen like a KTP600 and change the device in the project to a TP177A. The Basic Panels 1st Generation also have not all functions. The TP177A is also a linux based Panel with do not support all functions of a TP177B (WinCE). Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on