10/14/2018 3:53 PM | |
Posts: 5 Rating: (0) |
David, I understand this might be unrelated, but this is my first time here and I am facing commissioning deadline. I am using CONT_C in a function block. I call the FB in a Cyclic Program (OB32). when the PID is in manual I can change the Block CV by entering a manual value of 0-100%. The problem is starts when I put the loop in Automatic. It is a simple Flow control loop. As soon as I put the loop in Automatic, the loop becomes very unstable. Proportional gain is 0.1, Ti is 0 ms, PV_FAC=1. Derivative is also 0. SP=1100, PV (0-1800). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/15/2018 9:03:40 AMNew subject after splitting |
|
10/14/2018 3:56 PM | |
Joined: 12/18/2014 Last visit: 11/19/2024 Posts: 34240 Rating: (4263) |
Hello AutoGen_1560996, please don't post twice for the same problem. |
10/15/2018 9:09 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
|
Follow us on