9/21/2023 12:01 PM | |
Joined: 1/5/2021 Last visit: 10/15/2024 Posts: 13 Rating: (0) |
Sorry could I inserted those immediately. In the Zip file I've inserted the ZAP file from my TIA portal together with my LogoSoft file. The problem is pretty: We use a Logo! and HMI KTP400 to insert and control a view sensors within our machine. The main use of the HMI is to show which sensor gave an error, but it also controls the lubrication times and the time which is given for one cycle of the machine. When the operator shuts the machine down at the end of the day, and starts it back up the next morning. Then the HMI has lost all of the inserted times that the operator has inserted the day before. They are kept however inside the Logo! So just to keep off any confusion, the operator has to insert all of the values again each day which is annoying. Is there a solution for this so my HMI will keep the retentive values as well? I hope this is an better explanation. Kind regards, Job AttachmentSiePortal question.zip (383 Downloads) |
9/22/2023 12:05 PM | |
Joined: 1/5/2021 Last visit: 10/15/2024 Posts: 13 Rating: (0) |
just zero's |
9/22/2023 12:09 PM | |
Joined: 12/18/2014 Last visit: 10/19/2024 Posts: 33993 Rating: (4226) |
HHow did you define the input fields? Input only? |
Follow us on