12/21/2023 11:57 AM | |
Joined: 12/13/2014 Last visit: 6/5/2024 Posts: 144 Rating: (12) |
Let's see how many years takes correcting typo this time (LSC 8.4 online help, section "What is new in LOGO!Soft Comfort V8.4?") Btw, first time i noticed spelling error in LSC help. In the past, Siemens documentation seemed adamant about this.
Same online help in section "Configuring Ethernet connection, LOGO! to remote devices": Table in creating remote connections Claim: "LOGO!Soft Comfort supports to configure your local device to the following remote devices on the listed block types and their value range." According to table Logo 8.3 and lower (including 0BA8 standard) can connect with remote 8.4 to VX/VR memory area. Reality: New Diagram - select hardware: 8.3. Add NAQ and choose from properties Remote device. One can choose 8.4 in dropdown list, but can't choose VR/VX block type. ------------------------------------------------------------------------------------------ |
Last edited by: WWEE at: 12/21/2023 12:34:24Last edited by: WWEE at: 12/21/2023 12:35:09Last edited by: Jen_Moderator at: 12/22/2023 04:53:06New subject after splitting |
|
12/21/2023 3:23 PM | |
Joined: 6/11/2019 Last visit: 6/5/2024 Posts: 2201 Rating: (98) |
Comfort yourself, there are some hidden mistakes in German too... |
Follow us on