3/18/2022 7:05 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33168 Rating: (4098)
|
Import of a technical question via PM from the user Azalia.Az Hi dear expert, I do have a Windows 7 pro SP1 - 64 bit with LOGO Soft V8.3 installed. I can create a new project and do any moditications but when I want to download any project to PLC, I get java.lang.nullpointerexception error. Do you have any idea what might be the reason and what could be the workaround? I appreciate your help in advance. Thank you |
This contribution was helpful to2 thankful Users |
3/18/2022 7:25 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33168 Rating: (4098)
|
It's not my problem. I created the topic from a received PM. |
Follow us on