12/15/2010 12:53 PM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
as far as I've seen, it's nowhere documented but if you want to open a picture in Runtime through a shortcut for example on your desktop, make a new shortcut and use "C:\Program Files\Siemens\WinCC\bin\PdlRt.exe" "C:\yourprojectpath\yourprojectname\GraCS\yourPDLName.PDL" as Target in the shortcut properties. Similar to other software, it's possible that some extra startup commands exist also but I can't find any information about it. If you use this shortcut, WinCC will also activate RT if needed. If anyone has more info about this way of starting pictures in runtime through shortcut, I'll be glad to find out. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
6/7/2011 11:26 AM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Hi, Here I have created a new document about how to activate the WinCC runtime without opening the WinCC explorer and without configuring the autostart. This is very useful to avoid the operater to get into the configuartion level of WinCC. AttachmentHow to open runtime directly.pdf (5320 Downloads) |
_______________________________________________________________ |
|
This contribution was helpful to7 thankful Users |
6/7/2011 1:55 PM | |
Posts: 947 Rating: (45) |
string for autorun should write in regisrry (windows) as change Explorer, |
Follow us on